Other Parts Discussed in Thread: TAS5760M
Hello !
Firstable I want to apologize for my English ^^
Then, let's go for my interrogations :
I just bought an audio amplifier board for my raspberry PI, the main device of this board is TAS5756M.
The board manufacturer says that not any hybrid flow is used. So I suppose that the main board drive the component like a simple "DAC" by I2S.
Considering this, if I want to use the output in PBTL configuration, what am I supposed to manage on the DAC input signals ? I mean, if I make that both channel input signals are the same, what can prevent me from bridge output in PBTL configuration ? I don't see in the component datasheet any hardware configuration (by pull-up or pull-down or something else) to switch from BTL to/from PBTL. For example I don't find configuration pin like on the TAS5760M OR TPA3136.
I suppose there is a bit in an internal register configuration to "allow" PBTL mode, but I did not find in the datasheet which register has to be modify...
Thanks a lot for your answers,
Best Regards,
Jeremy