I have tested TPIC8101 with the following sensors in a real environment (engine at 2000-4000 rpm, under heavy load):
* Nissan 22060-56S10 (resonant, 1 wire) - functions very well. many hours of testing with no issue.
* Nissan 22060-30P00 (flat-response, 2 wire) - functions very well, surprised it actually worked. A few hours of testing with no issue.
* Toyota 89615-22040 (resonant, 1 wire) - extremely noisy, very poor knock detection performance. Using voltage divider ratio of 22 somewhat helps, and increasing p2p voltage to maximum, but still noisy (false knock reading) than the above two sensors. Changing centre frequency does not help. This was tested under light-load conditions.
The above observations was made by graphing knock level per ignition event over time.
my question is:
1) which sensor type is supported / not supported and
2) "The TPIC8101 only works with the resonant type knock sensor. We do not offer a device that works with the non-resonant type. " - http://e2e.ti.com/support/applications/automotive/f/26/t/118763.aspx - How did this conclusion come about?
Thanks.