Hi everyone,
I connect the adapter to PVDD. The leds are on (means the board sees the voltage), but in GUI the DC Bus Voltage showed 28.8 and the round button is grey. So I think, the GUI can not detect the DC Voltage of the board.
All the jumpers are on the right position and I wanna drive the stepper motor. Had/Has someone the same problem?
--- New: I think there is a shotcut or somthing like this. The FAULT button is on, when I enable the outputs AB CD (meaning turn /RESET_AB und _CD to normal option)
--- going on: Fault but no OTW, that means overcurrent or undervoltage. But if the case is untervoltage, the leds should not be turned on, so it is overcurrent.
in this post happend something similar: http://e2e.ti.com/support/applications/motor_drivers/f/38/p/109462/390682.aspx#390682
So my next step: measure the real current, then change the resistor?
Is a broken H or L bridge the reason?
--- Last for today: I measured direct on the pins of DRV8412, where the /FAULT and /OTW are HIGH, means no errors! All others are:
GND and AGND ok!
Vreg =3.3V
PWM_A..D=0.6V (switch s1, s2 in the middle)
GVDD_A..D=12V
PVDD_A..D=24V
Voltage on OC_ADJ= 1.1288V
BST_A..D=12V
The chip does not see any problem? Ok, I will continue with this issue. But it is nice, if somebody has any ideas.
Long