Hello TI E2E Community members,
I have a question regarding the DRV8842 (DC Motor Driver), configured as in this image. The DRV8842 H-bridge works when 4.3 V is applied first, and then the 12 V for the VM. However, when I have the 4.3 V node set to 0 V and apply VM, the nFault of the DRV8842 remains low even after the 4.3 V is applied. Is there supposed to be a specific order as to which pins should go high/low first?
Your help will be greatly appreciated. Thank you.