Hi,
I am trying to update the application code on a TAS1020B so it can configure the attached IDT AC'97 Codec for Mono Out rather than Mic In. I am having trouble using the DFUTest.exe utility to communicate with the TAS1020B. When the utility is executed, it responds with a "No DFU devices found" error. I have tried this with Windows Vista and Windows XP.
The device is detected by Windows and it loads its own USBAudio drivers rather than asking for the TI ones.
I am not using the EVM or Reference board. Its an embedded solution with the TI TAS1020B, 2-wire serial EEPROM, and an IDT AC'97 Codec.
Has anyone else had trouble with the DFUTest utility and Windows? If so, how were you able to overcome the issue?
Thanks
Harpreet