Hi,
I've built a serval of the remote volume module with the PGA2311. The power supplied from the Digital/Analog separated regulator with one 7VAC X 2 transformer. So they both D/A also from the same transformer but difference regulators for each part and the ground joined together.
I found that it working quite smooth and almost no noise there. But the mute not function very well all the time. Once I muted it and it never get back. I need to restart everything. This module working with the LM3875 as a passive preamp. Sometime it will mute itself even haven't click the Mute button. I am using the mute function inside the the chip.
I am using the same software and similar layout with the PGA2320 but nothing goes wrong.
I would like to know is it the problem of grounding or just happen in 2311? Should I put the 0.1uf cap between the DGND pin and the ground? What should I do? I built serval piece but problem still there... Please advise! Thanks!