This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254: Asking for the AIC3254 MCLK oscillator variation tolerance

Part Number: TLV320AIC3254


Hi Team,

Custome is designing AIC3254 on new platform. The MCLK is from 12.288MHz osicilator.
Here is the cusotmer's questions.
What is the AIC3254 AIC3254 MCLK input variation tolerence? 1%? 0.1%?


Thanks,
SHH

  • Hi, Scott,

    In general, we don't specify or characterize the tolerance for the clock inputs. A good assumption would be that  the typical tolerance of all clocks is +/- 2% maximum.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer