Other Parts Discussed in Thread: TPA3245, LCFILTER-CALC-TOOL
Hello!
I need to use TPA3255 in PBTL mode.
How do I make an output filter?
I have an inductor of 10 μH, 6.1 A, MA5172-AE Coilcraft
and film capacitors Film, 1 μF, 250 V,
In the document SLASEA8A, the PBTL scheme is drawn
OUTA, OUTC for one inductor and then a capacitor of 1μF
OUTB, OUTD to another inductor and then a 1μF capacitor
In the SLOU441 user manual, the output filter circuits for the PBTL mode are different.
Each output to its inductor and then a capacitor of 1μF
How to do it right?