This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5720A-Q1: Amplification for signal >20kHz

Part Number: TAS5720A-Q1
Other Parts Discussed in Thread: TAS5720M

Hi Team,

I am looking for an audio amplifier that can handle a signal bandwidth above the audio band, up to 75kHz. Is this a limitation that is set by the audio amplifier itself, or the output LC filter?

I took a look at the TAS5720A-Q1, and it look like the perfect device b/c it is class-D, mono output, and can produce >20W, but I am not sure if it can handle a signal up at 75kHz.. any insight you can provide would be greatly appreciated. 

Thank you for your support!

-Jared