This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3104: I cannot install AIC3104 GUI

Part Number: TLV320AIC3104


Hi,

When I double clicked setup.exe, it pop a window that The windows installer engine is corrupt,. To attempt to resolve this issue, please register the engine by regsvr32.exe on msi.dll.

I don't know how to run msi.dll, could you please help me? I looked for the answer in the e2e, looks like other people didn't meet this issue before. My OS is WIN10. 

  • Hi Wayne,

    I'm sorry to hear you are having trouble.  I  am glad to say we have seen this before, and the problem is easily solved.

    please right click on the setup.exe file and select "troubleshoot compatibility"

    You will also need to download the windows vista and Windows7 driver on the EVM product forlder (located in the software section)

    The driver folder contains two files:

    1. USB-MODEVM_vista&7.inf

    2. USB-MODEVM_WDM.inf

    Instructions for installing these files:

    USB-MODEVM_vista&7.inf Installation:
     To apply the contents of this file to a system's settings, right-click
     this file and choose "Install". If the device was plugged in before this
     file is installed, the device will need to be removed from the "Unknown
     Devices" class in the Windows Device Manager.

    ---------------------------------------------------------------------------------------------

    USB-MODEVM_WDM.inf installation:

    To apply the contents of this file to a system's settings, copy this file
     to %SystemRoot%\inf and reboot the computer. If the device was
    installed before this file is copied, the device will need to be removed
    from the "Unknown Devices" class in the Windows Device Manager.

    FYI the drivers were designed for windows 7 and vista, For windows 10,  you will need to disable signature confirmation, but otherwise they work flawlessly

    best regards,

    -Steve Wilson

  • Steve,
    Thanks for your reply.I still have problem to install it, I cannot find the file C:\windows\system32\drivers\NiViUsbK.sys according to the trouble shoot AN. Could you please help again?