Other Parts Discussed in Thread: ADS1118
There is a concern with the digital I/O leakage current on the ADS1018, which is rated at -10 to 10uA.
1.) Is the I/O leakage on the ADS1018/ADS1118 really +/-10uA?
2.) Is the leakage still present in the single-shot mode automatic shutdown scenario?
3.) Also, if the mux input is not activated, is the leakage still present or do all the pins leak (+/-10uA) whether they are actively connected to the mux/PGA regardless? Times four inputs the digital I/O could be up to 40uA if all the I/O leak regardless?