This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS5400: Does the batch number of ADS5400 affect the output?

Part Number: ADS5400


My customer used to use the 2013 batch number ADS5400. Later, he bought ADS5400 batch numbers for 2009 and 2010. Input the same signal,he found that the output waveforms of ADS5400 batches in 2009 and 2010 were different from those of 2013, and the static current of 2010 batches was more than 100 mA larger than that of 2013 batches.

Register updates are mentioned in the latest version of the ADS5400 datasheet. Will this affect output? What other reasons can cause this phenomenon? Any help would be much appreciated.