Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4
We have used AMC6821SQDBQRQ1 to control Fan speed using PWM out of this chip. Please note that we are using this chip in Software DCY mode, in which we have to set the duty cycle in DCY register We are not using auto temperature functionality or Tach mode this device. Please find attached snap of the schematic showing connection of this IC.
So far we are able to perform proper read/write operation with fan controller IC using system host controller (Sitara AM3505) through I2C.Following are the main configuration we are using:
Software DCY Control Mode [FDRC1:FDRC0] = [00]
TACH pin setup:
FAN-Fault-EN clear (‘0’)
TACH-EN clear (‘0’)
TACH-MODE set (‘1’)
PWM Output:
PWM-EN set (‘1’)
PWM_INV set (‘1’) as we are using N-FET
But , it seems that we are not getting any PWM Pulse. It is always with 100% duty cycle. We have checked the Therm-En bit of status register 3 is not set which can make this device to run with 100 % duty cycle.
I would request somebody to review the attached schematic and let us know if any issue with that , especially there are several input pins which are not connected and kept NC. Also let us know if we are missing any configuration setting.
Thanks,
Rizwan Hirnai