I want to use ADS1298RECGFE-PDK (REV B) without MMB0, I read some post about this problem (such as this), but it's not exactly for ADS1298RECGFE, I just want to check that whether the information I searched is correct or not.
There are some information I searched for power supply as the following:
1. Supply 5V on TP7.
2. Supply 3.3V on TP10.
3. Supply GND on TP8.
4. Install JP24 in 2-3.
5. Open JP4.
Is it correct for using ADS1298RECGFE-PDK without MMB0?