This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Gel files for CCSv4 OMAP4 Blaze ES2.2 XDS560v2 STM USB



I use
Emulator: Spectrum Digital XDS560v2 STM USB
Board : Blaze (OMAP4) ES2.2
CCS : setup_CCS_4.2.0.10018.exe
Script Release: 03172011_ccs_gel

Earlier for ES2.1(10252010_OMAP4430_es2.1_ccs_v2.zip) I was choosing the target
configuration
omap4430_ES2_freerunning_with_gel_wakeUp_topsim_xds560V2.ccxml

But, in the script release for ES2.2, I don't find the above target
configuration file. Can you please let me know the one I should be using.
  • Hi,

    Although I don't have a Blaze ES2.2 board with me, the closest configuration to the one you referred is in the package you referred (03172011_ccs_gel) is the:

    .\03172011_ccs_gel\config_M9\omap4430_ES2_freerunning_with_gel_wakeUp_topsim.ccxml

    Traditionally we leave for the customer to create his own target configuration file (the attached file contains a screenshot showing this), but the great number of GEL files in the OMAP4430 make this a rather complicated task.

    Therefore I modified the one above to include the SD XDS560v2 emulator connected via USB - the attached file also contains the ccxml file and a screenshot of this configuration launched in my Pandaboard ES2.1. Unpack the .ccxml file to the same directory shown above and link it to your project.

    Hope this helps,

    Rafael

    configuring_OMAP4430.zip