Hi,
I finally have u-boot.bin flashed into our custom board based on a C6A816x. Looking into the best options to debug the board bring up now. I know that CCS5 has some "Linux aware" features that appear to be able to understand gdb but I have not seen anything to confirm if I can load the u-boot ELF file and use it do to source level debug with JTAG and u-boot running on the target. Is this type of early board work still best done by a BDI-3000 type device?
Regards,
Brian