I'm attempting to upgrade to CCS5 from CCS4. But after I do, CCS5 can no longer connect to my MSP430BT5190.
My setup: Windows XP -> USB -> FET430UIF connected through JTAG to the MSP. With CCS 4.2.4 it works fine. CCS5 requires a firmware upgrade to the FET which seems to work but then when attempting to debug CCS5 can not connect:
MSP430: Error connecting to the target: Unknown device
If I downgrade the FET firmware and use CCS4 it is able to connect and debug without a problem.
I've tried powering my hardware via the FET and externally both with same results. (With CCS4 either power configuration works.)
Are there any differences between FET/JTAG settings between CCS4/CCS5 that may cause this? How can I troubleshoot?