Hi,
i am using an eclipsed based modeling tool which is able to generate C-Code. I want to install CCSv5 (5.1.0.09000) into this eclipse installation. Therefore i checked the button "Install CCS plugins into existing Eclipse installation" and added the correct path. The installation process seems to work fine for me, but after restart i can not select a CCSEdit or CCSDebug perspective. The "new Project" wizzard also don´t show an etntry for a CCS project. However, i checked the plugins in "Help->Install New Software->already instralled" and found that the plugins seems to be in place.
Can anybody tell me whats going wrong. Without having the perspectives and the project wizzard it is impossible to work.
Thanks for the help
Thomas Jung