Hi
CCSv4.2.5.00005
We have 5 XDS560v2s and two have stopped working. We can launch the debugger in CCSv4, but immediately after clicking the "connect" icon we get the error:
Error connecting to target
(Error -182 @ 0x0)
The controller has detected a cable break that is near-to-itself.
The user must connect the cable/pod to the controller.
(Release 5.0.429.0)
By switching out parts between working and non working systems, we've determined that the problem is the adaptor board PWC 5:2361 REV A (the 2 cm x 2 cm board with 7 chips on it that connects to the ribbon cable.
Are there any other debugging things we can try or do we have to order a new adapter?
The Spectrum Digital tool SdConfigEx does not appear to support the XDS560v2.
Cheers