Hi and thank you for looking at my problem.
version: CCSv4.2.4.00033
There is a previous post with a similar problem from Feb 2010, however the only response is sort of a "works for me" answer. I'm hoping to get more detailed help here.
My project resides on the C drive, but outside of the C:/StellarisWare location. It is basically a copy of the enet_io demo with the main difference that the project has actual copies of the third party Lwip. There are no linked files within my project.
My project compiles and a .out file is created, but no .bin file. Here is the output from the console:
<Linking>
'Finished building target: webIO_src.out'
' '
C:/Program Files/Texas Instruments/ccsv4/utils/gmake/gmake --no-print-directory post-build
"C:/Program Files/Texas Instruments/ccsv4/utils/tiobj2bin/tiobj2bin.bat" "webIO_src.out" "webIO_src.bin"
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/TMS470 Code Generation Tools 4.6.6/bin/ofd470.exe"
"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/TMS470 Code Generation Tools 4.6.6/bin/hex470.exe"
"C:/Program Files/Texas Instruments/ccsv4/utils/tiobj2bin/mkhex4bin.exe"
PAR/Dist.pm did not return a true value at -e line 320.
error: -image requires ROMS directive
' '
Build complete for project webIO_src
Thanks in advance for your help.
/Jason