Hi,
I am trying to do profiling on a C5515 hardware using CCSv4. DSP BIOS version of the project is 5.40.2.22. I have gone through wiki pages on profiling. In profle set up window,I could find only one option to profile all function for CPU cycles. I enabled that box. Inside properties,I could not find many options. Only CPU cycles are shown. And after enabling breakpoints and run the functions,in the profile window, I could see only a few DSPLib functions that were used in the code. Why cant I see the cycles for other functions?
But I can use profile clock. So is this the only option?
Plz help.Thanks
Regards,
James