Hi
I am trying to use the XDS200 to debug a TMS320DM642 device. I have emulation package 5.0.899. The emulator enumerates correctly in Device Manager, and passes the "Test Connection" activity in the CCS Target Configuration menu. However when I start a debug session I get :-
C64x: Error initializing emulator: (Error -2084 @ 0x0) Internal error: Missing or corrupt application file. Restart the application. If error persists, please report the error. (Emulation package 5.0.899.0)
I have CCS 5.1 - was unable to update to 5.3 due to update issues (seperate post) but I was able to update the TI emulation drivers.
I read on another post that this error may indicated that the DM642 is not supported by the XDS200 (even though SD recommended this emulator to me).
I welcome your comments
Thanks in advance
Malc