Hi,
I am facing build errors while trying to build dm6437 demo on code composer v5.
I referred to the following threads
http://e2e.ti.com/support/embedded/bios/f/355/t/151321.aspx
i have checked all the include paths and even edited as indicated in the previous thread. i have added the taregt name and type as -D compiler options as well.
however i am still getting the error, "cannot to open source file xdc/std.h"
what am i missing.? is thr a different version of cygwin tool for xdc 2.95 and xdc 3.22.? is that a problem?
i both installed initially but then i unstalled xdc 2.95, still i am facing the build issue with demo6437 with ccsv5, xdc 3.22 and DSP/BIOS 5.41
Please help