This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problems during ccs v3.3 and windows 7(32-bit)

"I want to generate a Code for my TI C2000 F28335 processor. Code Composer Studio is able to connect with the processor, but every time I try to build a model for it in Matlab I get following failures:

"The call to idelink_ert_make_rtw_hook, during the entry hook generated the following error: Could not connect to the board specified in Target Preferences block.

The build process will terminate as a result.

Could not obtain board configuration from Code Composer Studio™. Make sure that Code Composer Studio is installed and properly registered.

Error map is empty."

I use MatlabR2011b ,windows 7 and cc version 3.3. how can i solve this problem?

now how can i solve this problem? Thank you.

  • Hello,

    I would recommend contacting Mathworks for Matlab specific errors. They would have the most expertise. They can also confirm that the version of Matlab you are using is compatible with your CCS version.

    Thanks,

    ki