Mr/Ms,
Have been using MSP430 Launchpad for some time and find the TERMINAL very helpful. Decided to try the LM4F launchpad. I was using Windows 7 home premium. Downloaded all the needed stuff and then installed using ccs_setup_5.2.1.00018.exe, SW-EK-LM4F120XL-9453.exe, then the ICDI drivers. THen connected the Stellaris LP board, was able to load, run and change the blinky project and then the qs-rgb project. In the CCS IDE I could not find any TERMINAL as I had been using in CCS 4.2 with MSP430. However I started the Putty program (a communication program used in Windows 7 to substitute for Hyperterminal) and could communicate OK with the Stellaris Launchpad board.
My specific question is, does CCS 5.2.1 used with the Stellaris Launchpad have a TERMINAL feature that runs inside the CCS IDE, and if so, how to open its view and use it?