This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZdsp C5535 configuration

Hi, 

I need help configuring my eZdspC5535 starter kit board. I follow all the instructions on the Quickstart guide. When I get to the last part of the CCS configuration I get an error message "Error connecting to the target: (Error -151 @ 0x0) This utility failed to open the adapter for a custom emulator. The adapter returned an error. (Release 5.0.429.0)".

Note: My laptop is windows 8 and doesn't have a DVD reader so I installed CCS v4.2.4 through TI website. Also I installed the audio support after I made my first attempted to configure the device but even after I installed it I'm having this issue.

-Abdo