Hello,
We recently purchased 8 Spectrum Digital XDS510 USB Plus JTAG emulators. We are using them with three Concerto devices. We are running CCS v5.3.0.90. We are using both WinXP and Win7 64-bit OSes. We have been using the XDS510PP Plus and the XDS510USB (non-Plus) emulators for several months with our target boards with no issues. Once we switched to the XDS510USB Plus emulators, we are constantly getting error messages programming the M3 cores stating "DWARF information is corrupt". We have this issue with 4 of the 8 new emulators (we haven't tried the other 4). If we re-compile the M3 project with the error message, it usually programs the next time without without any issues, but the problem may move to one of the other M3 cores.
What is the cause of this? Are there any special settings that we can try? Or do these devices need newer drivers?