Hello,
I have a problem about the implantation of CCSV5 in Simulink (2012b)
The following print screens may show the problems more clearly:
Attached 3 files generated by printscreen.
In the file xmakefilesetup...
We created the upper user configuration ticcs_c6000_ccsv5 using the command Xmakefilesetup Note that the button 'Tool Directories does not appear in window, in contrast with the lower part which appears when we type in the command Xmakefilesetup on Matlab. We are therefore unable to execute the program ccs version5.
In the file board information...
We verified the connection of the board using the command ccsboardinfo . Matlab could not see the board.
In the file environmentcheck ...
We see that using the command checkEnvSetup Matlab could not find all required programs.
Thanks for your reponse.
Your answer would be very helpful for us.