Hello,
I have some troubles working with the CCS debugger.
My installation:
- Windows 7 Professional, Service Pack 1, 64-bit system
- Code Composer Studio version 5.5.0.00077
- Spectrum Digital XDS560V2 STM USB Emulator
- Evaluation board(s) BeagleBoard xM, BeagleBone, and EVM DM814x
Independent of the concrete evaluation board that is connected to the PC I can always establish a connection to the board, and also to a specific processor core. Downloading, starting and debugging any demo or example project is no problem - everything works fine. But each time I stop a debug session with "Terminate" (red square) CCS does not respond any more and I have to stop it violently with the Windows Task Manager. Since several weeks I see this phenomenon without a single exception and I don't know where to search for the root cause. Sometimes CCS creates a "dump file report" after a re-start - I sent them each time to "'CCStudio Error Reporting Service'". Hopefully it may help to identify the problem...
I experienced the same troubles already with the previous CCS version 5.4. Re-installation and the update to the version 5.5 didn't show any improvement.
What could be the reason for CCS crash?