This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hex2000 - setting the number of data items per line of hex output via -olength



Hi all,

I would like to use the hex2000 utility and set/restrict the number of data items per line of hex output.

The default max length is 20h. When calling hex2000 (cgtools 5.2.3) with -h, I get the option -olength to do this (this is not described in spru513c.pdf !!!).

When calling "\cgtools_5_2_3\bin\hex2000 -i -romwidth 16 -olength=10 myfile.out", it runs without problems and produces a single hexfile, but still with max. length of 20h !!

Does the option -olength work? How?

 

 

Edit by LH: moved to tools forum