This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer 4 downloading code to external flash

I am new to CCS and I am working on a custom DM648 based board. My understanding is that in earlier versions of CCS, external flash on the EMIF interface could be burned using the FlashBurn utility. As it is not compatible with CCS 4 and the new version wont be released until april, what would be a similar tool I could use in the meantime? Is there an integrated tool in CCS4 for that? Do I have to go back to CCS 3.3? Thanks for any feedback.

  • Hi Viktor,

    Currently Flashburn is not supported, like you mentioned. We have an integrated flash programming tool but it does not support all the ISA yet (like C6000). We are looking at expanding support but right now there is nothing yet

    ki