hello
i try to write and run a code for F28035 with CCS4 instead CCS3.3
whe i try to connect to exp. board the ccs4 give all time this message:
Error connecting to the target:
Error 0x80000200/-1047
Fatal Error during: OCS,
PTI_ERR_EMU_CLOSE Error Occured at 0x00000000
i check and select more times the right target and emulator XDS100V1 USB or XDS100V2 USB (why 2 emul.and what's the difference ?)
but not connect
the exp. board in CCS 3.3 latest working fine , in the same PC i have installed all ccs3.3 and ccs4 , and i try to run with another PC but the result it's the same : not connect .
thanks for help
Mario