I am having a problem with the XDS100 and starting my gel file. I get an error:
"Trouble Writing Memory Block at 0x1c40d00 on Page 0 of Length 0x4: Error 0x00000002/-1060 Error during: Memory, An unknown error prevented the emulator from accessing the processor in a timely fashion. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. .."
I get mostly the same mesages from the gel output:
Setup Cache (L1P = 32K) + (L1D = 0K) + (L2 = ALL SRAM)... [Done]
Setup PinMux... [Done]
All PSC Modules ON... [Done]
Setup PLL1 (Powering up PLL)... (DSP = 756 MHz + SYSCLK2 = 252 MHz + SYSCLK3 = 126 MHz + Onchip Oscillator)... [Done]
Setup PLL2 (Powering up PLL)...
Sometimes the last line about PLL2 doesn't show up but I the error is usually the same but the address may move a little bit (0x1c41a34) and sometimes after a few tries Composer actually crashes...
The same hardware, setup, and gel file work on another system. Well, at least I think its the same setup since something is obviously different!
Can someone point me in the right direction?