Hi,
Do I read correct CCS 6 is free with all functionalities and no (16k) code limit when used for developing for the CC3200 w MCU launchpad?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Do I read correct CCS 6 is free with all functionalities and no (16k) code limit when used for developing for the CC3200 w MCU launchpad?
Thanks.
Guy Dillen said:Do I read correct CCS 6 is free with all functionalities and no (16k) code limit when used for developing for the CC3200 w MCU launchpad?
I guess so, since I am able to build get_weather example program using CCS FREE version.
- kel
Yes, the CCS free license can be used without limitation with the on-board emulation on all non-MSP430 LaunchPads.
Thanks
ki