Hello.
I have just bought a three phase BLDS/PMSM motor kit with DRV8301 and the C2000 Piccolo F28035 MCU controlCARD. I have tried my motor in the preflashed GUI, and it spins perfectly.
I have now started to program in CCS, and I see that there are several labs that takes me through the process of identifying and spinning my motor. But, my problem is that the labs looks like they are specified for the F2802xF, F2805xF and F2806xF. I have the F28035, and wonder if I can use the same labs for my MCU?
Actually, I have already tried to complete some of the labs. I get to erase and load the new code into the chip, but after about 20seconds I get this error:
Trouble Reading Register PC:
(Error -1142 @ 0x0)
Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation.
(Emulation package 5.1.641.0)
Can anyone help me with this? Is it possible to run the lab on my F28035 MCU? If not, is there any other available labs? And if, why do I get the error above?
Thanks!