This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

error #10009 no input files

Hi,

I am using CS6.1 but always got this error while linking. But from the script, I think the objects are found by the linker. How could I know which file is missing?

the following is the linking process:

**********************************************

'Building target: Cyclone_POL.out'

'Invoking: ARM Linker'

"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.2/bin/armcl" -mv4 --code_state=16 --abi=ti_arm9_abi -O2 -g --display_error_number --diag_warning=225 -z -m"C:/Users/a0225311/Cyclone_WorkSpace/Cyclone_POL/Cyclone_POL.map" --heap_size=10 --stack_size=0x1D0 -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.2/lib" -i"C:/Users/a0225311/Cyclone_WorkSpace/Cyclone_POL/Debug" -i""C:/ti/ccsv6/tools/compiler/ti-cgt-arm_5.2.2/include" --reread_libs --warn_sections --display_error_number --xml_link_info="Cyclone_POL_linkInfo.xml" --rom_model -o "Cyclone_POL.out" "./PageControl.obj" "./PhaseControl.obj" "./adc.obj" "./adc_input.obj" "./adc_iout.obj" "./adc_temp.obj" "./adc_vout.obj" "./board_defaults.obj" "./command.obj" "./cyclone_global_variables_defs.obj" "./fan.obj" "./flash.obj" "./io.obj" "./io_setup.obj" "./isr.obj" "./load.obj" "./main.obj" "./pmbus.obj" "./pmbus_hardcoded_parms.obj" "./pmbus_read_cmds.obj" "./pmbus_utils.obj" "./pmbus_write_cmds.obj" "./profile.obj" "./sysinit.obj" "./tfa.obj" "../cyclone.cmd" "../HeaderFiles/cyclone.cmd" "../HeaderFiles/cyclone_headers.cmd" -l"libc.a"

<Linking>

fatal error #10009: no input files

 

Thanks,

Julie