This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
on a fresh configured PC (Win7) with a clean installation of CCS 6.1.1.00022 I discovered the following issue:
When trying to test the connection to the emulator in the following dialog:
I get the following error message:
I guess the reason for this is that the %boarddatafile% variable points to the default directory location somewhere in "C:\Users\sber\AppData\Local\Texas Instruments\CCS" and this path contains a white space...
(The configuration is saved in another directory without any white spaces in the path)
Is there a way to manually change this default path?
Thanks a lot,
Bernd
I think we finally figured it out - The "8.3 short file name support" was disabled during the clean installion of Win7 by our IT. Our IT has now to reinstall Win7 with enabled "8.3 naming schema" which should solve this issue with CodeComposer...
social.technet.microsoft.com/.../enable-83-short-file-name-support-to-windows-7
Hi Rafael,
I have had the same problem with both my home and office computer. It seems it only happens to the XDS510USB emulator. I find this discussion when I was trying to find a solution to it. But the soultion was simple: the test connection feature seems not working for the XDS510USB. The emulator works fine when I am trying to connect target and debug with it. It simplify cannot pass the connection test. I was on 6.1.1 first and then tried 6.1.0, but the same issue is there. Thanks
Han