Sorry if this is trivial, but I'm new to this whole game.....
I have the following two linker errors:
===================================================
error: cannot find file "usbstk5515bsl.lib" I have included a link to this library file in my root project directory, but the linker does not seem to find it....?? Do I need to copy the actual library file to the project directory? ============================================= fatal error: file "C:/Program Files/TI2/ccsv4/emulation/boards/usbstk5515_v1/lib/usbstk5515bsl.lib<usbstk5 515_led.obj>" has a Tag_Memory_Model attribute value of "2" that is different than one previously seen ("3"); combining incompatible files What is a Tab_Memory_Model and how do I set it? ============================================= Thanks for your help. MikeH