I bought a xds560 JTAG PCI EMULATOR KIT TMDSEMU560 from TI. When I used it to connect Davinci DM6446 EVM bought form SPECTRUM DIGITAL, it failed.
The message is :
Error connecting to the target:
Error 0x80002240/-183
Fatal Error during: Initialization, OCS, Control,
This error was generated by TI's USCIF driver.
SC_ERR_CTL_CBL_BREAK_FAR <-183>
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.
Does this emulator support the davinci dm6446 evm? What should I do to solve these problems