This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430F5659: error: unresolved symbol, first referenced

Part Number: MSP430F5659
Other Parts Discussed in Thread: MSP430G2553

Tool/software: Code Composer Studio

I am using msp430f5659 microcontroller. I am trying to interface lcd, uart but after build it gives error: unresolved symbol, reference first. I have read ti forums to resolve the error and i found that i am missing some library but not able to find which one. I have attached screen shots of my console, problem screen. Please suggest me which mistake i am making ?

  • harish yadav said:
    I am trying to interface lcd, uart but after build it gives error: unresolved symbol, reference first. I have read ti forums to resolve the error and i found that i am missing some library but not able to find which one.

    Harish,

    The unresolved symbol error is basically saying that main.c is referencing symbols clear_lcd, lcd_init, etc. but the linker cannot find a definition for it. The definition can either be in a C source file that gets compiled and linked as part of the project or in a library file that gets linked into the project. I don't have knowledge about the project/interface code you are working with to know where these symbols are defined, but I see that you have some source files in the /driverlibrary directory. Do those files contain the definitions for those symbols, I would imagine they should. Alternately the symbol definitions could come from a library but as to which library would be a question for the MSP device forum. 

  • I have defined all the symbols in their respective .c  files and declared them in .h file. I think my linker is not able to link all these files but why ? I am not able to resolve this problem please suggest something. I have read about these type of problem in ti forum but everywhere they says some file is missing in file search path. which file not able to find this ?

  • harish yadav said:
    I have defined all the symbols in their respective .c  files and declared them in .h file.

    Could you pick a couple of the unresolved symbols mentioned in the errors and attach the C source files where those functions are defined?
    Also please save the full output in the CCS build console to a text file and attach it here.

  • Note: this was cross posted to the msp forum.
  • Since as said it was related to msp430 forum so i posted it there also. I dont know whether it is related to msp or ccs forum.

  • hello,

    this is my lcd.h file:

    /*
     * lcd.h
     *
     *  Created on: Mar 21, 2017
     *      Author: acer
     */
    #include "inc/hw659.h"

    #ifndef DRIVERLIBRARY_LCD_H_
    #define DRIVERLIBRARY_LCD_H_

    #define lcd_RS   BIT1
    #define lcd_EN   BIT2
    #define lcd_D4   BIT3
    #define lcd_D5   BIT4
    #define lcd_D6   BIT5
    #define lcd_D7   BIT6
    #define lcd_DIR    P1DIR
    #define lcd_PORT   P1OUT
    #define lcd_PORT_MASK   (lcd_EN  | lcd_D4 |  lcd_D5 | lcd_D6 | lcd_D7)

    extern void lcd_cmd(char);
    extern void lcd_pulse(void);
    extern void lcd_init(void);
    extern void lcd_data(unsigned char);
    extern void set_cursor_pos(int,int );
    extern void clearport();
    extern void busychck(void);
    extern void clear_lcd(void);
    extern void display(unsigned char* word);



    #endif /* DRIVERLIBRARY_LCD_H_ */


    this is my 2 functions in c file in which error occurs:

    void set_cursor_pos(int row,int col)
    {
        char addr;
        if(row==0)
            addr=0x00;     //row 0 then addr=0x00h(RAM addr)
        else
            addr=0x40;  //row 1 den addr=0x40h
        addr |=col;     //add offset for column
        lcd_cmd(0x80|addr);  //set DDRAM addr for display
    }

    void clear_lcd()
    {
            lcd_cmd(0x01);   //CLEAR DISPLAY
                //_delay_cycles(1000);
            lcd_cmd(0x02);   //RETURN HOME
            //_delay_cycles(100000);
    }

    and i am attaching the console text file as u said.

    **** Build of configuration Debug for project rmu ****
    
    "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 
    'Building target: rmu.out'
    'Invoking: MSP430 Linker'
    "C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_16.12.0.STS/bin/cl430" -vmspx --data_model=restricted --use_hw_mpy=F5 --advice:power="all" --define=__MSP430F5659__ -g --printf_support=full --diag_warning=225 --diag_wrap=off --display_error_number --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 -z -m"rmu.map" --heap_size=160 --stack_size=160 --cinit_hold_wdt=on -i"C:/ti/ccsv6/ccs_base/msp430/include" -i"C:/ti/ccsv6/ccs_base/msp430/lib/5xx_6xx_FRxx" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_16.12.0.STS/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-msp430_16.12.0.STS/include" -i"D:/wrkspce/rmu/driverlibrary" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="rmu_linkInfo.xml" --use_hw_mpy=F5 --rom_model -o "rmu.out" "./main.obj" "./driverlibrary/adc.obj" "./driverlibrary/lcd.obj" "./driverlibrary/modbus.obj" "./driverlibrary/uarta1.obj" "../lnk_msp430f5659.cmd"  -llibmath.a -llibc.a 
    <Linking>
    
     undefined         first referenced
      symbol               in file     
     ---------         ----------------
     UART_GETSTRING    ./main.obj      
     UART_INIT         ./main.obj      
     UART_PUTSTRING    ./main.obj      
     build_querypacket ./main.obj      
     clear_lcd         ./main.obj      
    remark #10371-D: (ULP 1.1) Detected no uses of low power mode state changing instructions
     display           ./main.obj      
    remark #10372-D: (ULP 4.1) Detected uninitialized Port B in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
    remark #10372-D: (ULP 4.1) Detected uninitialized Port C in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
    remark #10372-D: (ULP 4.1) Detected uninitialized Port D in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
    remark #10372-D: (ULP 4.1) Detected uninitialized Port E in this project. Recommend initializing all unused ports to eliminate wasted current consumption on unused pins.
    
    >> Compilation failure
    makefile:147: recipe for target 'rmu.out' failed
     lcd_init          ./main.obj      
     set_cursor_pos    ./main.obj      
    
    error #10234-D: unresolved symbols remain
    error #10010: errors encountered during linking; "rmu.out" not built
    gmake: *** [rmu.out] Error 1
    gmake: Target 'all' not remade because of errors.
    
    **** Build Finished ****
    

  • harish yadav said:
    this is my 2 functions in c file in which error occurs:

    Is this in the lcd.c file? Could you please attach that file here and also attach main.c?

    Also please do a project rebuild and save off the contents of the CCS build console and attach here. The current build log only shows the link step.

  • hello,

    I am truncating my project to only lcd file and building it but showing the same error. Since my code was previously working on msp430g2553 but i am migrating to msp430f5659. Now i am trying to build my project again on msp430g2553 in this format, initially i define and declare function in header file but from now onwards i am trying to work in stdandar fromat. I am attaching the log file, main.c, lcd.h, hw659.h, driverlib.h file here for msp430g2553 mcu.

  • Harish,

    The issue here is a programming error and is unrelated to either the toolset or the device.  

    Looking at the build log I see that main.c is being compiled but lcd.c is not. Normally all C source files that are part of the project should be compiled and then the object files generated should be linked as part of the build process. In your project the C source files are main.c and lcd.c but only main.c was being compiled. I took a look at the source file lcd.c and saw the following:

    #ifdef DRIVERLIBRARY_LCD_H_
    #include"lcd.h"
    ...
    ...
    #endif

    Since DRIVERLIBRARY_LCD_H_ is not defined at that point in the source, the entire code in the file is assumed to not be valid, hence not compiled. If you move the #include "lcd.h" above the #ifdef line, then the symbol definition (and thereby rest of the code) will be valid and the lcd.c file will build. 

    Let us know if this helps resolve the issue.

  • thanx a lot AratiG,

    It worked for me......