This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IC2812 could not connect the CCS3.3 with SEED XDS510PLUS!!Please help!

When i connect the Ic2812 with the ccs3.3,it didn't work,and the failed message as follow:

Error connecting to the target:
Error 0x80000240/-171
Fatal Error during: Initialization, OCS,
This error was generated by TI's USCIF driver.

SC_ERR_REG_DETECT_CTLR <-171>
The wrong controller port value has been used.
A controller cannot be detected even though the
selected port does match the hardware configuration.
The standard 560 ports are 0x0, 0x1, 0x2 and 0x3.
The standard EVM ports are 0x0, 0x1, 0x2 and 0x3.
The standard DSK ports are 0x378, 0x278 and 0x3BC.
The standard 510 ports are 0x240, 0x280, 0x320 and 0x340.


Sequence ID: 0
Error Code: -171
Error Class: 0x80000240
I/O Port = 240

Board Name: F2812 SEEDXDS510PLUS Emulator
Cpu Name: TMS320C2800_0

Abort:  Close Code Composer Studio.
Retry:  Try to connect to the target again.
Cancel:  Remain disconnected from the target
Diagnostic: Run diagnostic utility.

and then press the retry,it changed failed message like this:

Error connecting to the target:
Error 0x80000200/-1037
Fatal Error during: OCS,
PTI_ERR_EMU_CLOSE Error Occured at 0x00000000


Sequence ID: 0
Error Code: -1037
Error Class: 0x80000200
I/O Port = 240

Board Name: F2812 SEEDXDS510PLUS Emulator
Cpu Name: TMS320C2800_0

Abort:  Close Code Composer Studio.
Retry:  Try to connect to the target again.
Cancel:  Remain disconnected from the target
Diagnostic: Run diagnostic utility.

PS:the power supply of IC2812 are normal.the input voltage 3.3v and 1.8v seem normal as before,but could not get a correct connection.JTAG signals are not correct.TRST  always kept low,TCK pin has no pulse for output,and  TDO also has no output signal.

Please help me,thanks a million everybody!

  • The following additional information might be helpful in diagnosing the issue:

    1) Is this a eZdsp board or custom board?
    2) Has this board ever connected to CCS 3.3 with this SEED emulator? Have you tried any other emulator, if available, with this board?
    3) Do you have the latest drivers from SEED installed for CCS 3.3?

    I would also recommend checking with SEED support directly as they may have additional suggestions.

  • I have a normal board,and it runs smoothly with the same SEED .So i think the board got some problems.

    Moreover,the board which does not work has ever connected to the CCS3.3 with the SEED emulator.I think the SEED should be normal.

    Thanks for your help.Would you give me any other suggestion?

  • If SEED has some emulator testing utilities included with their drivers for testing the JTAG scan chain connections, you could try running them. I don't have a SEED emulator but other emulation vendors have similar utilities, so I would imagine SEED would have something as well.

    You may also find this page helpful: http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems

    I would also suggest contacting SEED directly to see if they have other recommendations.