This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Missing a lot of basic commands from scripting console



Hi, 

I am new to Code Composer and the whole TI dev environment, so excuse any trivial questions. I am missing a lot of cmds on script console on my CCS installation.

I am using CCS Version: 4.2.0.09000 to connect to a C6A816x EVM. Everything works just fine and I can connect to different cores on the chip, step through code etc. 

But I am missing a lot of commands on the script console. I found that out when I was trying to run an example that required the use of loadRaw.  Did I miss something in my installation for cmds not to show up in script console? Or do I have to enable something? Below are the cmds that ARE actually present when I do a tab on the script console prompt. 

js:> 

cls               disableLog        enableLog         execCmdFile       help              listJSFiles       loadJSFile        loadKeyword       print             services          setWindowBuffer   unloadJSFile      unloadKeyword

 

Thanks. 

 

  • You do seem to be missing a lot of commands if that is all the commands you see after hitting tab. Could you try two things? First, your installation of CCSv4.2 is a beta install. Please update to the latest release (4.2.1.00004). Second, try using a new workspace.

    Thanks

    ki

  • Ki,

    I tried your suggestion but no luck. :(

    I upgraded to 4.2.1.00004 and even created a new workspace but I still do not get as many cmds on my scripting console. 

    Additionally here is what I observed. 

    - Another team member has my same old version(4.2.0.09000) of CCS and he gets all the cmds. Seems weird. 

    Is there a way to manually add these cmds so that I can use them in script console by copying it from my team mmeber's CCS installation. If so which files should I copy? 

     

    Thanks

     

  • Its resolved now. I guess something was wrong with my initial installation. I had to uninstall CCSv4 and install it in another location than the previous one. Now I see all the std cmds on scripting console. 

    Note that I had to install in a new location for this to work. Re-installing it in the same folder which I tried before did not work. I guess the initial uninstall did not clean everything up.