This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, all
As for TPS61256. Please see the attached waveform.
There are two type of start up - output voltage ramp.
Attached waveform, input is same 3.6V
Occasionally two type of output ramp happens.
Q1. Is it normal or abnormal ?
Q2. What is the triggar of 2nd ramp start (3.6 to 5V)
Best regards,