This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INTERNAL ERROR: C:\ti\ccsv5\tools\compiler\msp430_4.2.1\bin\acpia430.exe experienced a segmentation fault while processing

Other Parts Discussed in Thread: MSP430F4794

I received this error compiling a rather simple file.

This is the command line

:"C:/ti/ccsv5/tools/compiler/msp430_4.2.1/bin/cl430" -vmsp --abi=eabi --code_model=small --data_model=small -O0 --opt_for_speed=5 --include_path="C:/ti/ccsv5/ccs_base/msp430/include" --include_path="C:/Users/cbenson/Multi/Track-It 6700/inc" --include_path="C:/ti/ccsv5/tools/compiler/msp430_4.2.1/include" --advice:power="all,-2,-3,-5" -g --gen_acp_xref --gcc --gen_acp_raw --define=__MSP430F4794__ --define=MULTI --define=CCSV5 --verbose_diagnostics --diag_warning=225 --display_error_number --optimizer_interlist --remove_hooks_when_inlining --gen_opt_info=2 --printf_support=nofloat -k --c_src_interlist --asm_listing --output_all_syms --check_misra="required" --misra_advisory=suppress --misra_required=remark --preproc_with_compile --preproc_dependency="APDS-9300.pp" "../APDS-9300.c"

This is the line which caused the error:

	CmdReg.cmd = 1; // this is a command

The fault went away after turning OFF MISRA checking.
I can live without MISRA, but it is like having a second set of eyes looking over ones code.