This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI Compiler 7.4.2 doesn't like source files encoded in UTF-8 with BOM



Hi

If source files are encoded in UTF-8 with BOM (byte order marker), the CCS5 editor displays them correctly but the TI compiler (v7.4.2) gives an 'unrecognized token' error.

If 'UTF-8 (without BOM)' encoding is used, the source file compiles correctly, but the editor does not display it correctly.

This same problem was discussed in 2009 for CCS3:

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/99/p/7045/27350.aspx

Is there a solution for this problem yet?

Best regards

David