This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Possible compiler bug (msp430g2553)

Hello,

recently I ran into a problem while working with 64-bit integers on MSP430G2553. The code listed below does some manipulations with 64-bit unsigned integers. The problem only occurs on "cold start", i. e. after powering up the board, flashing the firmware and running it from CCS. However, this is a result of my attempt of minimizing the amount of code required to reproduce the problem; in my current project this problem happens every time the partucular piece of code is executed. Anyway, here is the code:

main.c:

#include <msp430.h> 
#include <stdint.h>

#include "test-file.h"

static test_struct test_struct_array[] = {
	{
		.data = 0xDEADBEEFDEADBEEF
	},
	{
		.data = 0xDEADBEEFDEADBEEF
	}
};

/*
 * main.c
 */
void main(void) {
    WDTCTL = WDTPW | WDTHOLD;

    f_init(
    	(test_struct *) &test_struct_array,
    	ARRAY_SIZE(test_struct_array)
    );

    LPM3;
}

test-file.h:

#ifndef TEST_FILE_H
#define TEST_FILE_H

#include <msp430.h>
#include <stdint.h>

#define ARRAY_SIZE(a)	(sizeof(a) / sizeof((a)[0]))

typedef struct {
	uint64_t data;
} test_struct;

void f_init(test_struct * d, uint8_t s);

#endif

test-file.c:

#include "test-file.h"

test_struct * t;
uint8_t c;

void f_b(uint8_t a) {
	volatile int b = a;
}

void f_a() {
	uint64_t a  = t[c - 1].data;
	uint64_t b = t[c - 1].data;
	//
	uint8_t i = 63;
	//
	do {
		f_b(1 && (a & ((uint64_t) 1 << i)));
		f_b(1 && (b & ((uint64_t) 1 << i)));
	} while (i--);
}

void f_init(test_struct * d, uint8_t s) {
	t = d;
	c = s;
	f_a();
}

Expected result and the problem

There is a breakpoint in the screenshot below. At this point, both a and b should be equal 0xDEADBEEFDEADBEEF. However, b is 0xFFFF847DDEADBEEF (upper 32 bits differ from time to time, so I guess these bits are kind of random). Screenshot:

When volatile keyword is added to the variable declarations, everything works as excepted.

Is this a compiler or code problem?

Optimization settings: 0 (Register optimizations)

Compiler: MSP430 Compiler Tools 4.3.5

CCS: 6.0.1.00040 

Regards,

-- Vlad