Hi,
I'm trying to re-build UBL for dm368 processor in CCSv4 enviroment.
I have the following error during linker operation:
'Building target: ubl_dm365.out'
'Invoking: Linker'
"C:/Programmi/Texas Instruments/ccsv4/tools/compiler/tms470/bin/cl470" -mv5e -g --diag_warning=225 -me --abi=eabi --code_state=32 -z -m"ubl_dm365.map" --warn_sections -i"C:/Programmi/Texas Instruments/ccsv4/tools/compiler/tms470/lib" -i"C:/Programmi/Texas Instruments/ccsv4/tools/compiler/tms470/include" --reread_libs --rom_model -o "ubl_dm365.out" "./CCS/NANDEraser/src/nanderaser.obj" "./CCS/NANDWriter/src/nandwriter.obj" "./CCS/NAND_ECC_Test/src/nandtester.obj" "./CCS/NORWriter/src/norwriter.obj" "./Common/src/device_nand.obj" "./Common/src/device.obj" -l"libc.a" "../CCS/UBL/UBL.cmd" "../CCS/UBL/ubl2bin.cmd" "../CCS/NORWriter/NORWriter.cmd" "../CCS/NAND_ECC_Test/NAND_ECC_Test.cmd" "../CCS/NANDWriter/NANDWriter.cmd" "../CCS/NANDEraser/NANDEraser.cmd"
<Linking>
"../CCS/UBL/ubl2bin.cmd", line 3: error: invalid option: -zero
"../CCS/UBL/ubl2bin.cmd", line 4: error: expecting filename, option, MEMORY, or
SECTIONS instead of "8"
error: cannot find file "inkerfill"
ERROR: argument to option -f ("value") is out of range
>> Compilation failure
C:\Programmi\Texas Instruments\ccsv4\utils\gmake\gmake: *** [ubl_dm365.out] Error 1
C:\Programmi\Texas Instruments\ccsv4\utils\gmake\gmake: Target `all' not remade because of errors.
Build complete for project ubl_dm365
Could someone help us?
Thanks in advance.
Alfredo