This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 4.1 release now available!

Guru**** 467431 points


CCS 4.1 release is now available:

Highlights

  • Support for Stellaris devices
  • Improved performance (most evident on multi-core devices)
  • Support for XDS100v2
  • Numerous fixes and enhancements

Improved performance includes:

  • Improved CCS start-up times (up to 50% improvement)
  • Speed and memory usage improvements when launching debug sessions for devices with many peripheral registers. This is especially evident on multi-core devices (up to 70% improvement)
  • Improved symbol lookup performance. This is primarily visible in situations where a large number of lookups are performed after a target halt
  • Improved memory footprint when loading large DWARF symbol files

Currently only a full CCS 4.1 installation image is available. A patch update for existing 4.0 users will be available in a few weeks.

Download is available from the CCS download site: http://tiexpressdsp.com/index.php/Download_CCS