Dear Sir or Madam
We are going to use TPS43061 Controller. We found that some results from WEBENCH design do not match with TPS4306x_BOOST_CALCTOOL_REVB.xls tools (and Datasheet calculation). For example, WEBENCH gives cross-over frequency 15kHz, Phase Margin 50°, Gain Margin 10dB (good margin).
We used component's value from WEBENCH design in TPS4306x_BOOST_CALCTOOL_REVB.xls and got cross-over frequency 8.7kHz, Phase Margin 53° and Gain Margin minus 9dB (excitation). It is not small mismatch, but completely different result.
So, which tools we should trust?
We tried to make a simulation model for this controller, but it datasheet does not have enough information:
1. Parameters of slope compensation signal
2. Parameters of Error Amplifier output: Does it sink current or source current or both and what is the its output current limits.
We would really appreciate your help