hi
it usually boot up failed frist time. after one or two on/off, it could boot up successfully.
why is it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shuai,
This is an unusual behavior. Does it fail to boot up each (first) time? Is it booting from NAND or SD?
Regards,
Divya
yes, each first time. it should boot from NAND, no SD inserted in.
There is another problem additionally, int the gui software, I want to save sollution persistently, however, once lightcrafter boot up, all saved sollution lost.
Hi Shuai,
Can you please upgrade the DM365 software booting from NAND by downloading the package, DLP LightCrafter Firmware and Software v1.1. Make sure the following versions are seen in the GUI,
DM365: v3.31, FPGA: v 2.4.39, MSP430: v2.5
Please let me know if the issue persists after the upgrade.
Save the solution as 'Default' to save the patterns in NAND flash and to run this solution when device boots up.
Regards,
Divya